GANTRY.PL.ERRWTHRESH
Description
If this value is not equal 0 and the position error GANTRY.PL.ERR is larger than this value, the drive will generate a warning.
If GANTRY.PL.ERRWTHRESH is set to 0 the warning is not issued.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-02-02-000 |
General Information
| Type | Read/Write |
| Description | Sets the position error warning level for Gantry Mode. |
| Units |
Rotary: counts, rad, deg, custom units, 16-bit counts Linear: counts, mm, µm, custom units, 16-bit counts See Position Units for details. |
| Range | Depends on units. See Position Range for details. |
| Default Value | 0 counts |
| Data Type | Float |
| See Also | AXIS#.PL.FB |
| Stored in Non Volatile Memory | Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
GANTRY.PL.ERRWTHRESH | 0x300E:3 (position unit scaling, uses axis 1 scaling) | 0x4 | INT | 1:1 | - | RW | False |